Bluetooth module for bed Made for • iPhone 4 • iPhone 4S • iPhone 5 • iPad 2 • iPad 3rd generation • iPad 4th generation • iPad mini • iPod touch 4th generation TABLE OF CONTENTS Connect to bed .3 Pairing Bluetooth .4 LED functions .6 How to download the App Software.7 How to use the App.8 Connect to bed Connect the BT2LIN box directly to the TD1 or TD3 bed by use of the enclosed cable (article number 0705835). On TD3 the box can slide on to the holder on the side of the TD. No other connection is needed. USB Input Power If you wish to enable the TWINDRIVE® actuator to go into lowest standby power, you can power the BT2LIN from a standard USB charger with MicroUSB connector (not included). Then the BT2LIN does not keep the TWINDRIVE in operational mode, but can wake it on command. Pairing Bluetooth Device Discoverable First time the device is powered up, and until the first pairing has been made, the BT2LIN box is visible in the bluetooth device list all the time. Once the first device is paired to the BT2LIN box, the box switches to non-discoverable mode after 5 minutes and is no longer visible to other devices. This is done to prevent unintentional usage from other devices. To connect additional devices to the BT2LIN box, power down and up the bed/box. Then the box is in discoverable mode for 5 minutes again. The box can be paired to up to 6 devices at one time, additional devices being paired will cause the first paired devices to be unpaired. Autoreconnection The BT2LIN box automatically reestablished the connection to the paired devices once they are within range and turned on. This reconnection can take a few minutes to take effect. iPod touch, iPhone, and iPad are trademarks of Apple Inc., registered in the U.S. and other countries. “Made for iPod touch”, “Made for iPhone,” and “Made for iPad” mean that an electronic accessory has been designed to connect specifically to iPod touch, iPhone, or iPad, respectively, and has been certified by the developer to meet Apple performance standards. Apple is not responsible for the operation of this device or its compliance with safety and regulatory standards. Please note that the use of this accessory with iPod touch, iPhone or iPad may affect wireless performance. The Bluetooth word mark and logos are owned by the Bluetooth SIG, Inc. and any use of such marks by Ascion, LLC is under license. Other trademarks and trade names are those of their respective owners. 2 3 4
Download PDF file